This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: How to test and verify the ADC converted data which is triggered by ETPWM?

Part Number: TMS570LC4357


Hi,

I'm using TMS570LC4357 HDK,

and I'm testing ADC1 channel 0 hardware trigger using EVENT group and trigger source is EPWM_EVENT_B.

Every time interrupt occur handler will get call and converted data will be around 2667(slightly difference)  always, even though for other channels which are connected to EPWM.

if i change the duty cycle to 0, then the connected channel's ADC value will change to 0.

why other channels ADC value is 2667. and how to verify?

Thanks and Regards,

Bharath

  • Hello Bharath,

    Your question: ADIN[0] is connected to external input, and other ADC channels are left unconnected (floating). But the unconnected ADC channels get the same sampled value as ADC channel 0. 

    The sampled value of a floating ADC channel is indeterminate. If you connect those unused ADC pins to GND, what are the sampled value for those channels? Please try to enable the sample capacitor discharge mode. This mode will discharge the sampling capacitor before starting the sampling phase of the next channel.

  • Thank you Wang,

    after enabling sample capacitor discharge mode unconnected channel values are below 100.