Part Number: MSP-EXP432E401Y
Other Parts Discussed in Thread: MSP432E401Y
Hi experts,
My customer is using MSP-EXP432E401Y, and suddenly the following error occurs and the software cannot be written.
Q: Could you please tell me how to solve this problem?
They tried the following, but it did not solve the problem.
- Check if the TMS and TCK jumpers are in place on LaunchPad. ......Recheck result: -615
→Refer to "Incorrect SWD header". - Lower TLCK from Target Configration. ......Recheck result: -615
→The "The JTAG TCLK Frequency" in Target Configration is lowered. - Check if JTAG Mode is set to "SWD Mode" in Target Configuration. ......Recheck result: -615
→Change JTAG/SWD/cJTAG Mode to "SWD Mode- ~~TDO" or "SWD Mode- ~~UART" in Target Configration. - Replace the USB cable. ......Recheck result: -615
- Use a different sample code to check the writing. ......Recheck result: -615
→Use "buttonled". - Set the device to the factory default. ......Recheck result: -615
→Refer to "Using SimpleLink MSP432E4 microcontrollers over the JTAG interface (Rev. A)"."5.3 Executing Unlock Sequence" and "6.2 JTAG Not Working After Software Was Loaded".
The F/W (user program created by the customer) that they wrote before seems to be working, and they can input commands and display data from the UART via USB on the XDS110.
The same phenomenon occurs when they connects this evaluation board to another PC for debugging.
Currently, I'm asking for confirmation that they can use an external emulator and to share the F/W that they originally wrote. I would appreciate it if you could tell me if there is another way to solve this problem.
Best regards,
O.H