Part Number: TMS570LS1224
Hi,
I want to implement FLA13 "Software test of flash sector protection logic" diagnostics at boot and run-time, appreciate if you can give me some direction.
Regards,
Abdul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1224
Hi,
I want to implement FLA13 "Software test of flash sector protection logic" diagnostics at boot and run-time, appreciate if you can give me some direction.
Regards,
Abdul
Hi Abdul,
The flash content is protected from modification. There is one register called Flash Bank Protection Register (FBPROT). When bit 0 of FBPROT register is zero, which is default value, the level 1 protection is enabled which means that writing to flash sector enable register is disabled. If the flash sector is enabled, the sector can not be erased and programmed.
You can check if the FBSE (flash bank sector enable register) is writable if the level 1 protection is enabled or disabled.