Part Number: MSP432E401Y
Hi,
What are the changes needed to configure this project to use a static address?
Thanks,
-Mike
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432E401Y
Hi,
What are the changes needed to configure this project to use a static address?
Thanks,
-Mike
Hi Mike,
Looking at Line 237 in the 'lwiplib.c' file in the "ethernet_with_lwip_MSP_EXP432E401Y_nortos_ccs" project, the default IP mode appears to be static already.
//***************************************************************************** // // The default IP address acquisition mode. // //***************************************************************************** static uint32_t g_ui32IPMode = IPADDR_USE_STATIC;
There are three options in 'lwiplib.h'.
//***************************************************************************** // // IP Address Acquisition Modes // //***************************************************************************** #define IPADDR_USE_STATIC 0 #define IPADDR_USE_DHCP 1 #define IPADDR_USE_AUTOIP 2