Hi Experts,
The Data Manual of the TMS570LC4357 mentiones a EMS 1.43 for Ethernet Errors. Table 6-46 says that "Any error reported by slave beeing accessed" will assert ESM 1.43.
As far as I understand, this would mean that any error in the Ethernet Modul (e.g. CRC Error, Physical Layer Fault...) will set ESM 1.43. What confuses me is, that neither the Reference Manu al nor the Safety Manual mentions that any error gets signaled to the ESM. For example: in the Safety Manual the Error Response for a CRC Error should be an interrupt.
(Q1) When exactly will ESM 1.43 be set and is there any way to configure this outside of the ESM?
Best regards,
Max