This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: UART RX DMA

Part Number: TMS570LC4357

Hi Wang, As per your earlier recommendation we used DMB instructions before the application reads the DMA buffers every time. But we are still seeing the cache and the RAM are not coherent and observing data misses. 

We are clueless on what we are supposed to do. But when the shared RAM region is cache disabled, the issue is not observed. But, running in cache disabled mode may impact the timing, so we were thinking, what exactly we need to do to resolve this problem.

When cache is disabled, we used below configuration.

Thanks,

Kishore

  • Hello Kishore,

    Can I have the link to the original post? Thanks

  • I did a test using invalidate the data cache, so the memory region becomes coherent. The CPU can read the updated data from SRAM.

    This is my example code:

    1. the data buffer is allocated to .sharedRAM which is write-back and write allocated

    2. the destination address of DMA transfer is in the section: .sharedRAM

    3. Assigned data to rx_buffer[] first before DMA transfer

    4. DMA transfer data from SCI RD register to rx_buffer[]

    5. When DMA transfer is completed, invalidate the cache

    6. check the memory content in CCS memory browser. The content is updated.

    /* dma control packet configuration stack */
    g_dmaCTRL g_dmaCTRLPKT;
    uint32 DMA_Comp_Flag;

    uint8 data_buff[128];

    #pragma SET_DATA_SECTION(".sharedRAM")
    uint8 rx_buffer[128]= {0}; /* receive buffer in sys ram */
    #pragma SET_DATA_SECTION()


    /* USER CODE END */

    int main(void)
    {
    /* USER CODE BEGIN (3) */
    #if ((__little_endian__ == 1) || (__LITTLE_ENDIAN__ == 1))
    uint8 src_addr_offset = 0; /* 0 for LE */
    #else
    uint8 src_addr_offset = 3; /* 3 for BE */
    #endif

    uint32 IDLECOUNT = 0, i;

    _mpuInit_();

    /* Reset the Flag to not Done*/
    DMA_Comp_Flag = ~0x55AAD09E;

    sciInit();

    for(i=0; i<16; i++){
    rx_buffer[i]= 0x55;
    }

    asm(" nop");

    for(i=0; i<16; i++){
    rx_buffer[i]= 0x5A;
    }

    /* Print header on SCI1 */
    sci_printf(" Hercule SCI RX DMA Example - Version %\n\r");
    sci_printf("**************************************\n\r\n\r");

    /* Enable CPU Interrupts */
    _enable_IRQ();

    /* Enable DMA */
    dmaEnable();

    /* Enable Interrupt after reception of data */
    dmaEnableInterrupt(DMA_CH0, BTC, DMA_INTA); /* DMA_CH0 is highest priority */

    /* - Populate dma control packets structure */
    g_dmaCTRLPKT.SADD = (uint32)(&(sciREG1->RD)) + src_addr_offset;
    g_dmaCTRLPKT.DADD = (uint32)(&rx_buffer[0]);
    g_dmaCTRLPKT.CHCTRL = 0; /* channel control */
    g_dmaCTRLPKT.ELCNT = 1; /* element count */
    g_dmaCTRLPKT.FRCNT = 16; /* frame count */
    g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
    g_dmaCTRLPKT.ELSOFFSET = 0; /* element source offset */
    g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
    g_dmaCTRLPKT.FRSOFFSET = 0; /* frame source offset */
    g_dmaCTRLPKT.PORTASGN = PORTB_READ_PORTA_WRITE;
    g_dmaCTRLPKT.RDSIZE = ACCESS_8_BIT; /* read size */
    g_dmaCTRLPKT.WRSIZE = ACCESS_8_BIT; /* write size */
    g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type */
    g_dmaCTRLPKT.ADDMODERD = ADDR_FIXED; /* address mode read */
    g_dmaCTRLPKT.ADDMODEWR = ADDR_INC1; /* address mode write */
    g_dmaCTRLPKT.AUTOINIT = AUTOINIT_OFF; /* autoinit */


    /* - setting dma control packets for transmit */
    dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT);

    /* assigning dma request: channel-0 with request line - 1 - RX*/
    /* DMA Request 28 is for LIN ( SCI1) Receive */
    /* Refer Data sheet - Default DMA Request Map section */
    dmaReqAssign(DMA_CH0, DMA_REQ28);

    /* setting the dma channel to trigger on h/w request */
    dmaSetChEnable(DMA_CH0, DMA_HW);

    /* Enable RX DMA */
    sciREG1->SETINT = (3 << 17);

    sci_printf("sci dma rx Example \n\r");

    //please input 16 chars from TeraTerm Terminal

    /* Wait for the DMA interrupt ISR to set the Flag */
    while(DMA_Comp_Flag != 0x55AAD09E){
    IDLECOUNT++;
    }
    coreInvalidateICDCByAddress(0x0807F000, 0x1000);

    asm(" nop");
    /* USER CODE END */

    return 0;
    }