Part Number: TMS570LC4357
Hi team,
In our application for TMS570LC4357 processor we are using DMA engines where we are using the DMA channel numbers for establishing the communication over DMA. While implementing some of the DMA features, we have observed issues.
1. To configure the triggering type we have observed that the registers are not getting updated as per the need. As per the TRM, HWCHENAS is used to configure the Hardware triggering whereas SWCHENAS register will be used for software triggering. But, it has been observed that HWCHENAS is getting configured properly but SWCHENAS register is not getting updated properly, even though we are on the privilege mode. Let me know how do we need to implement this logic so that, the required dma channel number we can configure for the required trigger type.

2. For configuring the dam channel priority also we would like to understand how we need to achieve this. As per the TRM, we have CHPRIOS and CHPRIOR registers for configuring the high and low priorities, but when we tried to configure the low it is not properly updating the required bits in that registers. Here also we would like understand how to achieve this so that we can configure the channel priority appropriately. For e.g. ch2 for low, ch5 for high, ch10 for high, ch15 for low.
Regards,
Shivam