Part Number: TMS570LC4357
Good morning,
We are experiencing some interference between different peripherals running with hardware triggered DMA on different MIBSPI interfaces and we having some trouble nailing down exactly what is going on with the configuration of DMA request lines, sources and channels on the TMS570LC4357.
Table 20.3 (DMA Request Line Connection) maps DMA request sources to request lines. It is not entirely clear to us what the meaning is of the index number on MIBSPI interfaces in the middle column of the table (DMA request sources) could you clarify this?
E.g. in table 20-3 DMAREQ[9] is shared by sources MIBSPI1[5] and MIBSPI3[5], what does the 5 signify in this case?
Also, the DMA section of the datasheet specifies the existance of 32 "DMA channels" and 48 "request lines" while the MIBSPI section specifies there are 8 channels and 16 request lines that can be used, what is the difference between these two? Ar are they the same and can we only use a subset for DMA channels/requests for MIBSPI?
Thanks for your help.