This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[CC1312R1F3RGZR] Can I use two DIO pins to drive an LED to get more drive strength?

Other Parts Discussed in Thread: CC1312R

I am trying to drive 8mA through a series resistor and LED and do not wish to use a transistor to do so because of cost requirements. I am wondering if I can use two DIO pins, (each with their own resistors) to drive a single LED so that I can get the required current I need. As of now, I can drive close to 8mA but am seeing a voltage drop on the pin when doing so. The IC I'm using is the CC1312R1F3RGZR.