Part Number: TMS570LS0432
Hallo, as you see, i test the BQ boaurds using the software Battery Managment Studio to measure the temperature of the cells. and it's works propably!
Know i try to write a code to read the measurement, And i followed the same steps as in the screen shoot.
+ Ist number 5 in the screenschoot is just to set the bit AUX_ADC_GO in the register CONTROL2, or there is something else?
WriteReg (0, CONTROL2, 0x02 , 1 , FRMWRT_SGL_NR ); // START ADC Measurement, bit Name: AUX_ADC_GO, B1
+ to read the temperature ( absolut voltage) , should i read the registers, AUX_GPIO1_HU, AUX_GPIO1_MU and AUX_GPIO1_LU, right? or should i read another rigisters?
ReadReg(0, AUX_GPIO1_HU, fram_uncorrect , 3 , 0 , FRMWRT_ALL_R ); // bytes AUX_GPIO1_HU , AUX_GPIO1_MU and AUX_GPIO1_LU
I'm waiting for your responce. Thanks for your time.