Part Number: TM4C123FH6PM
Other Parts Discussed in Thread: SYSBIOS, , TM4C123GH6PM, EK-TM4C123GXL
Hello Everyone,
I am trying to port FatSDRaw example to use a USB Mass Storage Device.
There is no direct example for usb using fatfs directly so I ported the usb example from 129 to 123 first.
I can read the usb stick and open files and read their contents using fatfs calls.
This gives me confidence that the issue I am facing is not USB related.
However, when I try to create a new file I get a system abort.
To test If I was doing something wrong I took a FatSDRaw example for 129 and changed SPI parts to USBMscFat and I can create new files without issues.
I have FatFS enabled on my cfg file as well.
I traced the abort to the following function call by using the debugger.
ff.c -> f_open -> line 2509 "dw = GET_FATTIME();"
GET_FATTIME(); is a define that calls get_fattime();
diskio.c get_fattime calls ti_mw_fatfs_getFatTime();
which is implemented in pem4f.c file created by xdc tools.
Contents of the function are following:
Int32 ti_mw_fatfs_getFatTime(Void)
{
time_t seconds;
UInt32 fatTime;
struct tm *pTime;
seconds = time(NULL);
pTime = localtime(&seconds);
/*
* localtime() sets pTime->tm_year to number of years
* since 1900, so subtract 80 from tm_year to get FAT time
* offset from 1980.
*/
fatTime = ((UInt32)(pTime->tm_year - 80) << 25) |
((UInt32)(pTime->tm_mon) << 21) |
((UInt32)(pTime->tm_mday) << 16) |
((UInt32)(pTime->tm_hour) << 11) |
((UInt32)(pTime->tm_min) << 5) |
((UInt32)(pTime->tm_sec) >> 1);
return ((Int32)fatTime);
}
on the seconds = time(NULL); line the time function is called.
time_t ATTRIBUTE time(time_t *tout)
{
UInt32 t;
/* Seconds_get() returns number of seconds since Jan 1, 1970 00:00:00 GMT. */
t = ti_sysbios_hal_Seconds_get();
#if defined(__ti__)
/*
* TI time() function returns seconds since 1900, so add the number
* of seconds from 1900 to 1970 (2208988800).
*/
t += 2208988800;
#endif
if (tout) {
*tout = t;
}
return (t);
}
On line t = ti_sysbios_hal_Seconds_get();
Seconds_get(); function in Seconds.c file is called.
UInt32 Seconds_get(Void)
{
UInt32 curSeconds;
UInt32 seconds = 0;
curSeconds = HWREG(HIB_RTCC);
seconds = curSeconds - Seconds_module->refSeconds +
Seconds_module->setSeconds;
return (seconds);
}
This is where I get the abort.
It accesses the Hibernation RTC register so my gut feeling is somehow RTC is not enabled and goes to hardfault.
Did anybody experience a similar issue before that they can help me?