Other Parts Discussed in Thread: AWR6843, MMWAVEICBOOST, AWR6843ISK
Used MCAL: 01.04.01.00.GA MCAL for AWR6843 Device
Used HW: MMWAVEICBOOST and AWR6843ISK
In Can_MCan.c, the following code is present (line 243 and more) :
Dem_ReportErrorStatus(CAN_E_HARDWARE_ERROR, DEM_EVENT_STATUS_FAILED);
Dem_ReportErrorStatus holds a uint16 as first parameter whereas CAN_E_HARDWARE_ERROR is a uint32 set to 0xFFFFFFFFU.
The compiler shows the following warning :
warning #70-D: integer conversion resulted in truncation