Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
I ran this example with pin changed for my TMS570LS1224 board.
training.ti.com/hercules-how-tutorial-using-nhet-generate-pwm
I had enabled HET1 driver and configured NHET[16] in halcogen code generator with duty cycle 60% and time period 1000uS. Also enable the output direction corresponding to pin16.
After which I had generated the code and included in the CCS project ( same workspace folder) . In sys_main.c , I had written the following code,
/* USER CODE BEGIN (0) */
#include "het.h"
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
#include "system.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
hetInit();
while(1) {}
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
void esmGroup1Notification(int bit)
{
return;
}
void esmGroup2Notification(int bit)
{
return;
}
void pwmNotification (nhetBASE_t * nhetREG, unsigned pwm, unsigned notification)
{
return;
}
void edgeNotification (nhetBASE_t * nhetREG, unsigned edge)
{
return;
}
/* USER CODE END */
I am getting the following error message while compiling the code.
#20 identifier "nhetBASE_t" is undefined sys_main.c /watchdog/source line 89 C/C++ Problem