Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0332: Errata issues for SSWF021#45 and DCC#24

Part Number: TMS570LS0332
Other Parts Discussed in Thread: HALCOGEN

The code solution for the issue SSWF021#45 in errata SPNZ226A can be generated in HaldCoGen tool. 

We are not using the DCC module, so the issue DCC#24 is not affecting us.

Question: Does the code fof HaldCoGen tool for resolving SSWF021#45 consider the issue DCC#24?

Note: The code of HalCoGen is the same spna233b has. The function that use the DCC is called check_frequency(uint32 cntl_clksrc).

the previous function uses Single Shot mode.