Part Number: TM4C129XNCZAD
Dear all TI Engineers,
I find a cheap supply of this nice board EasyMx PRO v7 for Tiva with an onboard TM4C129XNCZAD MCU:
https://www.mikroe.com/easymx-pro-tiva
It also shows that it has an onboard 10 pins Cortex Debug Connector.

It comes to my mine that my MSP432P401R LaunchPad has a TI XDS 110 Debugger/Programmer on board

which is very similar to the 10 pins Cortex Debug Connector on the above mentioned EasyMx PRO v7 for Tiva.
Now my question is:
If I power my MSP432P401R LaunchPad + its XDS 110 Debugger/Programmer, connect it to the 10 pins Cortex Debug Connector on EasyMx PRO v7 Tiva, and then develop, debug and programme its TM4C129XNCZAD MCU from within Code Composer Studio v10.3, do you think that this combination of hardware and software IDE is 100% compatible with each other?
I want to receive your opinions before I decide to place an order. Thanks in advance.