This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am unable to import any example from C2000Ware directory. I am using CCS Version: 10.3.1.00003 with C2000Ware (3.04.00.00).
The following message is displayed when I try to import:
I have also tried using project import option but no project is listed as shown below:
Please help in fixing this issue.
Just figured out that the issue was with the installation folder name. I had done manual installation earlier and the created folder name was : "C2000Ware_3_04_00_00". However the required name is "C2000Ware_3_04_00_00_Software". I removed the existing installation and tried installing from within CCS. This time the created folder had correct name and I am able to import projects.