Other Parts Discussed in Thread: TM4C123GH6ZXR
Hi E2E,
We have a customer who is interested in using a TI device instead of STM32 and looking for an MCU that will work with a touchscreen LVDS. Do we have any solutions available with the following specifications?
Requirements/Specifications
- Memory: 24 kilobytes currently being used (not including the graphical user interface)
- Touchscreen 4 pins
- LVDS: need an intermediate to convert LVDS to the MCU protocol
- Support a backlight for the screen
- LED
- Audio specifications for a amplifier that can work between 20Hz-80Hz as strong as STM32F446ZCJ6
- Speaker output for a beep sound
- Must be able to read heat sensor
- Must support external storage
- UI library for LCD-TFT screen
Secondary requirements/specifications:
- Interface to connect RFID reader
- USB interface (1 or 2)
Regards,
Carlo