This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: LAUNCHPADXL TM320F28379D some boards Loading program wrong

Part Number: LAUNCHXL-F28379D

Hi, 

I am using the LAUNCHPADXL TM320F28379D. I took one of them and I practice the Lab exercises until Lab 7 without problems. However I took a couple of new evaluation boards, same version VER:2.0 and same USB probe XDS100V2, also the same CCS version, and I am having problems when loading the program Lab7. 

After Debug (exactly the same Debug configuration) I cannot see any signal in the expected pins, also when I terminate the debug session and I try to debug again, I am getting a verification error:

A pop-up window error "Load program Error" File C:\workspaceDelfinoLocal\Lab7\Debug\Lab7.out: a data verification error ocurred, file load failed. 

Also a message in the console:

C28xx_CPU1: File Loader: Verification failed: Values at address 0x00000@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: C:\workspaceDelfinoLocal\Lab7\Debug\Lab7.out: a data verification error occurred, file load failed.

I have checked the silicon version on the chip and they same to be the same version C: $4C the one not working , $7C the one working. 

It is curious because I can load without problem Lab 6 in all the evaluation boards I have. 

Have anyone seen this erro before?

Any help would be very appreciated. Thanks in advance. 

Best regards 

Rafael