Hi,
In TRM manual, it mentioned “if the application has enabled high-resolution period control (HRPCTL[HRPE]=1), the duty cycle
must not fall within the restricted range. Otherwise, there will be undefined behavior on the ePWM output.”
Does the “duty cycle” means duty value after CMPA (CMPB) before Dead Band calculation or after Dead Band calculation ?
In HR period enabled mode, if the PWM output is configured with dead band, in case, the CMPA(CMPB) is bigger than 3 cycles,
but the pulse width after dead band becomes smaller than 3 cycles. Does this case work?
I really appreciate your help.
Wenjing