Other Parts Discussed in Thread: C2000WARE
Hi expert,
I want to know whether F280025 support multiple slave address or not?
and which part can tell this?
I look through TRM of MSP432P401M, and found there is 4 register so support 4 slave address.
"The registers UCBxI2COA0, UCBxI2COA1, UCBxI2COA2, and UCBxI2COA3 contain four slave addresses. Up to four address registers are compared against a received 7- or 10-bit address. Each slave address must be activated by setting the UCOAEN bit in the corresponding UCBxI2COAx register. Register UCBxI2COA3 has the highest priority if the address received on the bus matches more than one of the slave address registers. The priority decreases with the index number of the address register, so that UCBxI2COA0 in combination with the address mask has the lowest priority."
https://www.ti.com/lit/ug/slau356i/slau356i.pdf
I did not find similar information on F280025. so C2000 still can not support multiple slave address.am I right?
If so , can we support that by SW method?
BR
Emma