Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH, , C2000WARE
Hi,
i´m downloading the code with JTAG. With CCSv7 the debugging session is working and the programm is running fine. Then after i switch power off/on, nothing happens. It seems like flash is not working anymore.
Two years ago it was working because in production they are flashing with the first version (v1) i made with uniflash. Now with the newest version (v2) they say they cant flash anymore. Its working if they flash first the older version (v1) and then flashing v2 over v1. Then its running fine. But when only flashing v2 its not working. (Uniflash project is the same, nothing changed)
So if i tried to flash an already flashed controller it is working, but flashing a blank controller, it not working. Like i said in beginning, i can deug the with ccs when flashing into blank controller. But after power cycle its not running.
Did something change? What is wrong?
Please help.
Best regards
Willi Konrad






















-->