Part Number: C2000WARE
Other Parts Discussed in Thread: SYSCONFIG
Hi I just downloaded and installed the new C200o ware, as i need some of the new features in there.
But i also found a small bug.
Note: I am using a f28002x device, but based on the location of the error i asume it is general for more processor tyeps.
To trigger bug:
- In sysconfig setup a CAN device
- Give The Can device another name than the default myCAN..
- Build project.
You get an error:
"generated/board.c", line 247: error #20: identifier "myCAN0_BASE" is undefined 1 error detected in the compilation of "generated/board.c".
It appears that the BASE name has become hardcoded to `myCan0_BASE` in one line of the generated board.c
the problem line is:
// // Start CAN module operations // CAN_startModule(myCAN0_BASE);
Fortunately the fix is easy
--- driverlib/.meta/can/can.board.c.xdt.old 2021-10-21 10:32:27.137006700 +0200
+++ driverlib/.meta/can/can.board.c.xdt.new 2021-10-21 12:36:21.239429700 +0200
@@ -57,7 +57,7 @@
//
// Start CAN module operations
//
- CAN_startModule(myCAN0_BASE);
+ CAN_startModule(`instance.$name`_BASE);
% let instancePinmux = instance[nameOfModule];
% let solution = instancePinmux.$solution;
% let peripheral = system.deviceData.peripherals[solution.peripheralName];