Part Number: TMS320F28334
I am using a FT2232D USB Interface to program the flash on the on-board TMS320F28334. I can connect using CCS on my laptop but get an error when using another computer.
The message is:
Error connecting to the target
Error 0x80000240/-604
Fatal error during: Initialization, OCS,
The error was generated by TI's USCIF driver
SC_ERR_LOB_ANY_LOAD <604>
A required dynamic library could not be installed.
The attempt to load or install the library failed.
Any help with this would be appreciated.