This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: C2000Ware: F28069.cmd FPUTABLES : origin = 0x3FD590,

Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE

Hi,

please check the origin address of the following line twice for the 28069.

Fullscreen
1
FPUTABLES : origin = 0x3FD590, length = 0x0006A0 /* FPU Tables in Boot ROM */
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

Source: C2000Ware_4_00_00_00/device_support/f2806x/common/cmd/F28069.cmd

  • Hello,

    I checked the boot ROM source code and the FPU Tables are allocated as shown below.  The ROM source code can be found here:

    C:\ti\c2000\C2000Ware_4_00_00_00\libraries\boot_rom\f2806x\v1_1\rom_sources\lnk

    I will file a bug report against the F28069.cmd file. 

    Regards

    Lori