Part Number: TMS320F28386S
Other Parts Discussed in Thread: C2000WARE
Hi,
i build project based on cm_common_config_c28x and enet_lwip projects.
i work on my custome board.
in project cm_common_config_c28x i made change for the ethernet MII IOs as in my board.
in project enet_lwip i made change for the IP address and subnet mask for my PC subnet.
i connect the TMS320f28386s to marvel switch soppurt MII protocol.
one of the switch input ethernet connect to my PC.
i run chrome set the ip of the device and i see the webserver inside the tms320f28386s. -
169.254.146.10 - TMS320f2838s IP configured
169.254.146.255 - PC IP
open command window for ping test ping -n 5 -l 1500 169.254.146.10
the result is:
sometimes i get result and sometimes not
its looks that is not stable
advice