Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
The schematic is as shown. when I am soldering the LS07 (HEX BUFFER) IC the PWM signal at gpio1-6 is becoming 0. when I am removing the buffer the signals are coming fine 0-3.3 V pulses. Also, I checked the buffer circuit only by lifting the input pin and giving PWM in from the experimenter kit, the output is coming fine. Can u suggest what could be the problem?


without buffer ic pwm 1(gpio 00)