This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: Automatically disconnection of communication with PC

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: MOTORWARE

Dear All,

I'm running custom hardware with LAUNCHXL-F28069M. I'm trying to to use lab01b for custom hardware verification.  The communication get lost soon after PWM get activated and i'm not able to control the process anymore.

The following error messages are shown below :

C28xx: Error: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 9.4.0.00129)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting.  There may still be breakpoint op-codes embedded in program memory.  It is recommended that you reset the emulator before you connect and reload your program before you continue debugging

I tried every suggestions from previous topic, but there is no result here.

Could you give me advices ?