This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Flash kernel for TMS320F28388D

Guru 14870 points

Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE

Hi,

1) I was able to find sample code for CPU2 and CM flash_kernel in C2000Ware, but not for CPU1. Has flash_kernel for CPU1 been released?

2) The following is an excerpt from the ReadMe of the SerialFlashProgrammer. I think I should specify Kernel with the -k option. Which file should I specify?
(ReadMe mentions serial_flash_programmer_f2838x.exe, but the sample only had serial_flash_programmer.exe)

Thanks,

Koki

  • Hi Koki, 

    The CPU1 flash kernel is available in C2000Ware v4. The path is C2000Ware_4_00_00_00\driverlib\f2838x\examples\c28x_dual\flash_kernel for CPU1-CPU2 and C2000Ware_4_00_00_00\driverlib\f2838x\examples\c28x_cm\flash_kernel for CPU1-CM. 

    The hex file generated when building the CPU1 project is what should follow the -k parameter. Using the serial_flash_programmer.exe in C2000Ware v4 will wowrk for F2838x. 

    Thanks, 

    Anu