This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: C2000 I2C pull-up resistor

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: PCA9554A

Hello,

I'm using LAUNCHXL_F28379D to control an IO expansion chip PCA9554A. I use GPIO104 and GPIO105 as SDA and SCL with 4.7kOhm pull-up resistors. However, I observed the following waveform on SDA and SCL.

What I didn't expect is the rising edge of these signals. I thought the 4.7kOhm pull-up resistor should generate a quite sharp rising edge but looks like it is actually a slow rising edge. I checked my circuit and there is no capacitor on these two signals. Then, I removed PCA9554A and the waveform didn't change. So, my question is why the rising edge is slow? Thanks!

Best regards,

Yang