Part Number: TMS320F28069
C2000 Team,
We have a customer observing something unexpected on the I2C Clock pin and the same kind of thing on a GPIO pin.
They looked at the I2C Clock and saw a spike on the rising edge. They scoped a different pin, configured as output, toggling with GPIO_writePin(), and see the same spike. (This is an F28069, and they have modified DriverLib from F2837x to support the F28069.) On the GPIO pin, the only thing connected to that trace is a 100 kOhm pull-up.
I’m attaching a couple scope plots so you can see what I mean. Is this something familiar?
Thanks,
Darren