Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi everyone,
I would like to use a single-ended 3.3V levle clock on pin X1.
In the datasheet i see this sentence: "Crystal oscillator input or single-ended clock input. The device initialization software must configure this pin before the crystal oscillator is enabled. To use this oscillator, a quartz crystal circuit must be connected to X1 and X2. This pin can also be used to feed a single-ended 3.3-V level clock." but there is no other information on the datasheet or on the TRM.
I don't understand if it's necessary to start the singled-ended clock after software initiliazation, or anithing else. Indeed generaly we want a stable clock before the POR.
Regards