This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: support for 8 FSIRX ports?

Part Number: TMS320F28388D

I'm reviewing Fast Serial Interface (FSI) documentation to plan out a multi-controller architecture. Document SPRACR6-Distributed Power Control Architecture With Multiple
MCUs Over FSI includes

Section 5.1 - Star Connection

"F2838x MCU supports 8 FSIRX ports and, hence, this topology can work up to 8 slave devices in the
DPCA system. Thus, in a solar string inverter application one F2838x can control the DC/AC inverter
stage as a master device and then 8 F28002x or F28004x MCUs..."

(Fig. 15 from SPRACR6 - April 2020)

Looking through documentation on the F2838x, "SPRUII0C – MAY 2019 – REVISED FEBRUARY 2021" there is only mention of (2) Rx and (2) Tx.
Will there be a F2838x in the near future with (2) FSI-Tx and (8) FSI-Rx?