This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello TI
Now We have a problem. When the SPI speed is 2.5M, the data is normally received, but when it reaches 5M, there is dislocation. The data received at 10M communication speed is chaotic.
What is the theoretical maximum SPI reception speed of this processor?
SPI2 interface slave machine only receive not send
Hi Rain,
The max speeds are noted in the datasheet.
Internal clock prescalers must be adjusted such that the SPI clock speed is limited to the following SPI clock rate:
Master mode transmit 25-MHz MAX, master mode receive 12.5-MHz MAX
Slave mode transmit 12.5-MAX, slave mode receive 12.5-MHz MAX.
Please note that the speeds also depend on the signal integrity of your PCB design.