Part Number: TMDSHVMTRINSPIN
Other Parts Discussed in Thread: CCSTUDIO, MOTORWARE
I have got TMDSHVMTRINSPIN board and testing it today. I've checked all connections based on the documents "GUI Quick Start Guide: InstaSPIN_FOC_F2806xM" and "HVMTR Rev 1p1 Hardware Quick Start Guide". I tried both following:
v. J2
1. For DC bus input (recommended): Do NOT Populate J2 and a. connect 50-350V DC supply from BS6 to BS5
2. For AC input: Populate J2 Bridge-Middle 5
a. connect banana cable from BS5 to BS1
b. connect AC power cord to P1
So, whenever I just start InstaSPIN_FOC_F28069xM, I receive this message:
Restarting Program Model...
Initializing target : C:\ti\guicomposer\webapps\InstaSPIN_FOC_F2806xM\appConfig.ccxml
Connecting target: Texas Instruments XDS100v2 USB Emulator_0/C28xx
sun.org.mozilla.javascript.internal.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error connecting to the target: emulation failure occurred (<Unknown source>#14) in <Unknown source> at line number 14Restart Completed.
I tried connecting to the controller using CCS, and the target configuration can recognize the target there, but, I can not run InstaSPIN-FOC successfully.
Can you please help me with this issue?