Part Number: BOOSTXL-POSMGR
Hi,Lori
I used the CCS project of F280049C, which had successfully read encoder data before, to modify the protocol part to meet nikon encoder reading data, but the encoder did not respond.I understand that when I change the Tamagawa encoder to nikon encoder, I only need to modify part of the agreement.So I'm now modifying the function uint16_t PM_tformat_setupCommand(uint16_t tformatDataID, uint16_t eepromAddr,uint16_t eepromData,Uint16_t crcSend), and also get waveform, but it seems that the encoder does not respond.What is the reason for this?

(1)SPI's frequency is already 2.5MHZ;
(2)The instructions seem to be right, and the protocol looks like this:

Best regards
Johnson Alanl