Hi,
I am using TMS320F28388D, and i need to generate 3 phase pwm.
So I configured epwm1 as master and epwm 2,3 as slaves.
I need 40 KHz Switching frequency, so i configured TBPRD as 1250.
TBCLK is 100 MHz and counter mode is up down count.
The counter TBCTR will be changing from 0 to 1250 and 1250 to 0 right.
Now at what rate the TBCTR will be changing. Because when i measure epw1regs.TBCTR through CRO it's time period is 30 msec. Why it is 30 msec?
Whatever I measured is the right way for checking TBCTR or any other way is there to check the frequency of up down counter.
Thanks & Regards,
Saikumar.