This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: Inaccuracies in CMPSS Example 1

Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: C2000WARE

Hi.
I downloaded the example, ran it and it works. However, I have one concern about the program.According to the program description there should be a signal on the GPIO14 OUTPUTXBAR3 output that reflects the trip signal (J8 74 or J8 72 - it depends if you search by OPXBAR3 or GPIO).

According to the program description there should be a signal on the GPIO14 OUTPUTXBAR3 output that reflects the trip signal (J8 74 or J8 72 - it depends if you search by OPXBAR3 or GPIO). On the GPIO15 output EPWMB (J8 73).

In the kit documentation it says EPWM8B on GPIO32 (J8 71). OUTPUTXBAR3 is located together with GPIO26 (J8 74).

And the program itself works with the setting:
EPWM8B - J8 73
OUTPUTXBAR3 - J8 74

A question strikes me, is this a documentation error or a program error? As I wrote, the program runs and works for me, but I treat the thread as a place to report a noted bugs.