This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV425EVM: Design help recommendation

Part Number: DRV425EVM
Other Parts Discussed in Thread: DRV425

Hi Experts,

Good day. Seeking your assistance on this query:

hello i have purchases the DRV425evm, i am using it in a project to detect the magnetic field of cables used in residental homes. the microcontoller i am using is the arduino uno r3 and it has a insufficents ADC i was wondering based off the other questions which is recommended as i would like to use it for digital filtering and the DRV425evm is being used in a differential mode. for the filtering i would need to isolate the 60hz signal and i understand a bandpass filter would be best for this application however signal processing is not my strong suit, what would you recommend? meaning i have two. do you think you can assist me with this?

Thank you.

Regards,
Archie A.