This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fill option using command file and Gel options

Hi,

I want to fill the memory with ESOP0 and check for code crash scenario.

  1. To fill SRAM i am using gel option in code composer (Using Gel->Initialize memory map->Fill_F28335_RAM_with_ESOP0).
  2. To fill FLASH i am using 'fill' option in linker command. Ex: FLASHG      : origin = 0x308000, length = 0x008000, fill=0x7625. I am able to fill the Flash uing 'fill' option under Page 0 and it is compiling properly.
  3. The same way I am able to use 'fill' option for RAM under page 0, but the same i am not able to fill RAM under page 1. Its giving error as shown in below snapshot.

SRAM (RAML4, RAML5, RAML6 and RAML7) under Page 1 (with ERROR)

SRAM (RAML0, RAML1, RAML2 and RAML3) under Page 1 (with NO ERROR)

Simillarly i want to fill other places (Other than RAM and FLASH) like ZONE0, ZONE6, ZONE7A under Page 0. I tried similar to filling Flash under page 0. It compiled, but at that memory i am not able to find 0x7625, still its showing 0xFFFF. Please let me know how to fill at other locations other than RAM and FLASH.

Thanks & Regards

Vishnu

 

 

 

 

 

  • Hi,

    Please respond to this mail. If this is not the right forum, please move to appropriate forum.

    Also please let me know how to move the query from one fourm to other forum.

    Thanks & Regards

    Vishnu Beema

  • I cannot see your snapshots. Can you try to sent them again, or place the snapshots in a pdf and attach this file.

    Thanks

     

  • Hi,

    Please find the snapshots.

    • Through GEL script (Using Gel->Initialize memory map->Fill_F28335_RAM_with_ESOP0) I could able to fill RAM with ESTOP0. Below is the snap shot.

     

    • Similarly i tried to fill the FLASHH under PAGE 0 with ESTOP0. This is also working fine. Below is the snapshot.  

     

     

     

     

     

     

     

     

     

     

     

     

     

    • Even the same is working for RAML0 with Pop-up window saying "Warning: Because this program contains initialized RAM data it may run successfully under Code cComposer Studio but not as a standalone system".

     

    • But for ZONE6 under PAGE0 there is not error, (but a pop-up window with above warning). Still I am not finding any ESTOP0 code at ZONE6 location.

     

     

    • Now using same 'fill' option, if i try to fill FLASHB underPAGE1 I am getting several errors. This is applicable even to RAML4, RAML5, RAML6, RAML7 and ZONEB. Below is the snapshot

    warning: specified address lies outside memory map
    error: DEFAULT memory range overlaps existing memory range FLASHA
    error: DEFAULT memory range overlaps existing memory range CSM_RSVD
    error: DEFAULT memory range overlaps existing memory range BEGIN
    error: DEFAULT memory range overlaps existing memory range CSM_PWL
    error: DEFAULT memory range overlaps existing memory range ADC_CAL
    error: DEFAULT memory range overlaps existing memory range OTP
    error: DEFAULT memory range overlaps existing memory range IQTABLES
    error: DEFAULT memory range overlaps existing memory range IQTABLES2
    error: DEFAULT memory range overlaps existing memory range FPUTABLES
    error: DEFAULT memory range overlaps existing memory range ROM
    error: DEFAULT memory range overlaps existing memory range RESET
    error: DEFAULT memory range overlaps existing memory range VECTORS
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: DEFAULT memory range overlaps existing memory range VIRTUAL
    error: errors encountered during linking; "./Debug/rtl_test.out" not built

    • But for RAMM0 and RAMM1 under PAGE1 its giving a different error as shown below.

    "error: placement fails for object "$fill000""

     

    Please let me know why, when i try to fill the ESTOP0 code unde PAGE1, only causing this problem. Also please find the command file. (Rename .txt to .cmd)

    /*
    // TI File $Revision: /main/10 $
    // Checkin $Date: July 9, 2008   13:43:56 $
    //###########################################################################
    //
    // FILE:	F28335.cmd
    //
    // TITLE:	Linker Command File For F28335 Device
    //
    //###########################################################################
    // $TI Release: DSP2833x/DSP2823x C/C++ Header Files V1.31 $
    // $Release Date: August 4, 2009 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file, 
    // add the header linker command file directly to the project. 
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within 
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2833x_Headers\cmd
    //   
    // For BIOS applications add:      DSP2833x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2833x_Headers_nonBIOS.cmd    
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the 
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper 
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2833x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2833x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2833x_headers\cmd to the
       library search path under project->build options, linker tab, 
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28335  
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
        Notes: 
              Memory blocks on F28335 are uniform (ie same
              physical memory) in both PAGE 0 and PAGE 1.  
              That is the same memory region should not be
              defined for both PAGE 0 and PAGE 1.
              Doing so will result in corruption of program 
              and/or data. 
              
              L0/L1/L2 and L3 memory blocks are mirrored - that is
              they can be accessed in high memory or low memory.
              For simplicity only one instance is used in this
              linker file. 
              
              Contiguous SARAM memory blocks can be combined 
              if required to create a larger memory block. 
     */
    
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       ZONE0       : origin = 0x004000, length = 0x001000     /* XINTF zone 0 */
       RAML0       : origin = 0x008000, length = 0x001000     /* on-chip RAM block L0 */
       RAML1       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L1 */
       RAML2       : origin = 0x00A000, length = 0x001000     /* on-chip RAM block L2 */
       RAML3       : origin = 0x00B000, length = 0x001000     /* on-chip RAM block L3 */
       ZONE6       : origin = 0x0100000, length = 0x100000,fill=0x7625    /* XINTF zone 6 */ 
       ZONE7A      : origin = 0x0200000, length = 0x00FC00    /* XINTF zone 7 - program space */ 
       FLASHH      : origin = 0x300000, length = 0x008000     /* on-chip FLASH */
       FLASHG      : origin = 0x308000, length = 0x008000     /* on-chip FLASH */
       FLASHF      : origin = 0x310000, length = 0x008000     /* on-chip FLASH */
       FLASHE      : origin = 0x318000, length = 0x008000     /* on-chip FLASH */
       FLASHD      : origin = 0x320000, length = 0x008000     /* on-chip FLASH */
       FLASHC      : origin = 0x328000, length = 0x008000     /* on-chip FLASH */
       FLASHA      : origin = 0x338000, length = 0x007F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x33FF80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x33FFF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL     : origin = 0x33FFF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
       OTP         : origin = 0x380400, length = 0x000400     /* on-chip OTP */
       ADC_CAL     : origin = 0x380080, length = 0x000009     /* ADC_cal function in Reserved memory */
       
       IQTABLES    : origin = 0x3FE000, length = 0x000b50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008c     /* IQ Math Tables in Boot ROM */  
       FPUTABLES   : origin = 0x3FEBDC, length = 0x0006A0     /* FPU Tables in Boot ROM */
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */        
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
       
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       RAML4       : origin = 0x00C000, length = 0x001000     /* on-chip RAM block L1 */
       RAML5       : origin = 0x00D000, length = 0x001000     /* on-chip RAM block L1 */
       RAML6       : origin = 0x00E000, length = 0x001000     /* on-chip RAM block L1 */
       RAML7       : origin = 0x00F000, length = 0x001000     /* on-chip RAM block L1 */
       ZONE7B      : origin = 0x20FC00, length = 0x000400     /* XINTF zone 7 - data space */
       FLASHB      : origin = 0x330000, length = 0x008000     /* on-chip FLASH */
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */ 
     
    SECTIONS
    {
     
       /* Allocate program areas: */
       .cinit              : > FLASHA      PAGE = 0
       .pinit              : > FLASHA,     PAGE = 0
       .text               : > FLASHA      PAGE = 0
       codestart           : > BEGIN       PAGE = 0
       ramfuncs            : LOAD = FLASHD, 
                             RUN = RAML0, 
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL     PAGE = 0
       csm_rsvd            : > CSM_RSVD    PAGE = 0
       
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM1       PAGE = 1
       .ebss               : > RAML4       PAGE = 1
       .esysmem            : > RAMM1       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA      PAGE = 0
       .switch             : > FLASHA      PAGE = 0      
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
       IQmathTables     : > IQTABLES,  PAGE = 0, TYPE = NOLOAD 
       
       /* Uncomment the section below if calling the IQNexp() or IQexp()
          functions from the IQMath.lib library in order to utilize the 
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM 
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD 
       {
       
                  IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
       
       }
       */
       
       FPUmathTables    : > FPUTABLES, PAGE = 0, TYPE = NOLOAD 
             
       /* Allocate DMA-accessible RAM sections: */
       DMARAML4         : > RAML4,     PAGE = 1
       DMARAML5         : > RAML5,     PAGE = 1
       DMARAML6         : > RAML6,     PAGE = 1
       DMARAML7         : > RAML7,     PAGE = 1
       
       /* Allocate 0x400 of XINTF Zone 7 to storing data */
       ZONE7DATA        : > ZONE7B,    PAGE = 1
    
       /* .reset is a standard section used by the compiler.  It contains the */ 
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */ 
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
       
       /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */
       .adc_cal     : load = ADC_CAL,   PAGE = 0, TYPE = NOLOAD
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    
    

     Thanks & Regards

    Vishnu Beema