Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: DRV8311HEVM,
Hi,
I am trying to get the LAUNCHXL-F280049C working with the DRV8311HEVM board for motor control. I have tried using the DRV8311xEVM InstaSPIN Universal GUI, but despite running through all the board configuration & steps, the firmware fails to control the motor correctly.
So I am instead now trying to run through the univeral motorcontrol lab examples to adapt and build the firmware myself, so I should at least have debug access to see what is going on.
However, when I try to debug (and flash) my built application, I get the following error:
C28xx_CPU1: GEL Output:
RAM initialization done
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: Warning: Failed unlocking device (zone 1) after reset.
C28xx_CPU1: Warning: Failed unlocking device (zone 2) after reset.
C28xx_CPU1: Error occurred during flash operation: Unable to get file info from algorithm
C28xx_CPU1: Error occurred during flash operation: No algorithm has been loaded in which to look up "_exit"
C28xx_CPU1: Error writing the init algorithm. Flash algorithm returned error code. Operation cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\stephen.crumpler\workspace_v11\universal_motorcontrol_lab_f28002x\Flash_lib_DRV8316RT\universal_motorcontrol_lab_f28002x.out: Load failed.
C28xx_CPU1: Error occurred during flash operation: Unable to get file info from algorithm
C28xx_CPU1: Error occurred during flash operation: No algorithm has been loaded in which to look up "_exit"
It looks like the flash is locked some how, presumably by the firmware loaded by the DRV8311xEVM InstaSPIN Universal GUI?
Any idea how I can get this unlocked?
Thanks.