This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Compiler Announcement: Release version 22.6.0.LTS available for C2000/CLA



TI is pleased to announce a new C28/CLA compiler version 22.6.0.LTS which includes the following new features.

New features:

  • C28 performance improvements:
    • interrupt save/restore efficiency improvement
    • reducing register spilling
    • keeping global float/double variables in registers
    • additional if-conversion use cases
    • RTS library routine fmodf() now has faster tmu, relaxed fp_mode implementation using __fmodf intrinsic
  • CLA performance improvements:
    • support enabled for generating MMACF32||MMOV32
    • more efficient MRn loads of unsigned short 
  • New option --fp_single_precision_constant treats unsuffixed floating point constants as 32-bit
  • Hex tool: new options --boot_align_sect and --boot_block_size=size

For more details, please visit the download page for C28 compiler version 22.6.0.LTS