Part Number: TMS320F28388D
Hello.
I use processor TMS320F28388 .
I use PWM in my work.
It generates the desired signal.
And i have quetion.
How to programmatically disable PWM immediately?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Hello.
I use processor TMS320F28388 .
I use PWM in my work.
It generates the desired signal.
And i have quetion.
How to programmatically disable PWM immediately?
You can use TZ module to disable the PWM immediate
I have read about the tripZone module.
But I didn't find a function to disable PWM outputs.
//
// Trip Zone module related APIs
//
//*****************************************************************************
//
//! Enables Trip Zone signal.
//!
//! \param base is the base address of the EPWM module.
//! \param tzSignal is the Trip Zone signal.
//!
//! This function enables the Trip Zone signals specified by tzSignal as a
//! source for the Trip Zone module.
//! Valid values for tzSignal are:
//! - EPWM_TZ_SIGNAL_CBC1 - TZ1 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC2 - TZ2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC3 - TZ3 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC4 - TZ4 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC5 - TZ5 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC6 - TZ6 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCAEVT2 - DCAEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCBEVT2 - DCBEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_OSHT1 - One-shot TZ1
//! - EPWM_TZ_SIGNAL_OSHT2 - One-shot TZ2
//! - EPWM_TZ_SIGNAL_OSHT3 - One-shot TZ3
//! - EPWM_TZ_SIGNAL_OSHT4 - One-shot TZ4
//! - EPWM_TZ_SIGNAL_OSHT5 - One-shot TZ5
//! - EPWM_TZ_SIGNAL_OSHT6 - One-shot TZ6
//! - EPWM_TZ_SIGNAL_DCAEVT1 - One-shot DCAEVT1
//! - EPWM_TZ_SIGNAL_DCBEVT1 - One-shot DCBEVT1
//!
//! \b note: A logical OR of the valid values can be passed as the tzSignal
//! parameter.
//!
//! \return None.
//
//*****************************************************************************
static inline void
EPWM_enableTripZoneSignals(uint32_t base, uint16_t tzSignal)
{
//
// Check the arguments
//
ASSERT(EPWM_isBaseValid(base));
//
// Set the trip zone bits
//
EALLOW;
HWREGH(base + EPWM_O_TZSEL) |= tzSignal;
EDIS;
}
//*****************************************************************************
//
//! Disables Trip Zone signal.
//!
//! \param base is the base address of the EPWM module.
//! \param tzSignal is the Trip Zone signal.
//!
//! This function disables the Trip Zone signal specified by tzSignal as a
//! source for the Trip Zone module.
//! Valid values for tzSignal are:
//! - EPWM_TZ_SIGNAL_CBC1 - TZ1 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC2 - TZ2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC3 - TZ3 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC4 - TZ4 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC5 - TZ5 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_CBC6 - TZ6 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCAEVT2 - DCAEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_DCBEVT2 - DCBEVT2 Cycle By Cycle
//! - EPWM_TZ_SIGNAL_OSHT1 - One-shot TZ1
//! - EPWM_TZ_SIGNAL_OSHT2 - One-shot TZ2
//! - EPWM_TZ_SIGNAL_OSHT3 - One-shot TZ3
//! - EPWM_TZ_SIGNAL_OSHT4 - One-shot TZ4
//! - EPWM_TZ_SIGNAL_OSHT5 - One-shot TZ5
//! - EPWM_TZ_SIGNAL_OSHT6 - One-shot TZ6
//! - EPWM_TZ_SIGNAL_DCAEVT1 - One-shot DCAEVT1
//! - EPWM_TZ_SIGNAL_DCBEVT1 - One-shot DCBEVT1
//!
//! \b note: A logical OR of the valid values can be passed as the tzSignal
//! parameter.
//!
//! \return None.
//
//*****************************************************************************
static inline void
EPWM_disableTripZoneSignals(uint32_t base, uint16_t tzSignal)
{
//
// Check the arguments
//
ASSERT(EPWM_isBaseValid(base));
//
// Clear the trip zone bits
//
EALLOW;
HWREGH(base + EPWM_O_TZSEL) &= ~tzSignal;
EDIS;
}
//*****************************************************************************
I see PWM signals being disabled here only due to external signals.
I want to disable and enable PWM programmatically.
how to do it?
You mean you want to use SW to disable and enable?
What do you mean by SW?

I have PWM configured. And I want to programmatically turn on the output signals and then turn them off.
There is a SW FRC for the TZ module. it is a register (driverlib function that you can call ) and it will disable your EPWM by TRIPing it.