Part Number: TMS320F28388D
Hello
I am using both cores for my applications and using TI driverlib examples.The external crystal oscillator is 20MHz.
In the device.h file, define the micro #define USE_20MHZ_XTAL, which configures the core to run at 200MHz.
Do I need to configure the clock for core2 also, or is that taken care of by the void Device_init (void) function in the device.c file of the core?
Thanks in advance