Part Number: TMS320F280049
Champs,
My customer is using the following post-steps to generate .bin file.
"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/ofd2000.exe" "${CG_TOOL_ROOT}/bin/hex2000.exe" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe"
The problem is about the address after begin address.
If we directly program the .out file, the next 6*16bit would be filled with 0. But if the .bin file is programed, the next 6*16bit is filled with 0XFFFF.
The minor difference would cause a data check failure in customer's firmware update routine. If there any configuration that can be done to assign to fill with 0XFFFF or 0X0000?
Thanks,
Brian