Part Number: TMS320F28384D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
On behalf of customer.
PCB is in layout and working on the EMIF.
Regarding the pull-up resistors on the EMIF bus, I was planning to enable the GPIO pull up resistors for the EMIF data bus. This excerpt [shown below] leads me to believe that I cannot do that, but instead must use external resistors. Please confirm.
In document TMS320F2838x Real-Time Microcontrollers With Connectivity Manager SPRUII0D – MAY 2019 – REVISED JULY 2022 , Tables 12-21 through 12-24 mention address becoming valid and address becoming invalid. I understand address becoming valid but I am confused by address becoming invalid. Does that mean that the address bits are no longer driven and become tristate.
If the address bits are still driven, would they not remain unchanged until they become valid for the next memory access? Do the address signals have the GPIO internal pull-up? If so, should they be enabled? If not, should they have external pull-up resistors?

Does TI have an eval board that used the EMIF bus? If so, did that design have pull-up resistors on the data bus? I do not see any timing diagrams for asynchronous memory read and write that show timing information for when the DSP drives and releases the data bus with regards to Data Bus Parking.