Part Number: LAUNCHXL-F280039C
Other Parts Discussed in Thread: SYSCONFIG, , C2000WARE
Hi,
I'm using SysConfig in CCS 12.
I'm using LAUNCHXL-F280039C, its pinout can be seen at https://www.ti.com/lit/ml/spruj30/spruj30.pdf?ts=1659627276281&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FLAUNCHXL-F280039C
When configuring Sysconfig, specifically in ANALOG PinMux, the field A10/B1/C10 is triggering a warning when the selcted option is A10/B1/C10/40, as seen in the picture below:

The warning stated 'Not pinned out', if I hover over the warning it states that this pin is not pinned out in the Launchpad that I'm using and according to the pinout documentation link I added before, the pin A10 is pin 64 in J7 would you please let me know what is the meaning of the warning?
In the board view, I can see that pin 64 in J7 header is assigned to A11/B10/C0, as well as pin 27 in J3. I understand then that it might be an issue with the board configuration information:

Additionally, I have read https://www.ti.com/lit/an/spracx3/spracx3.pdf?ts=1659690064075 but I find the document rather a quick use document rather than a detailed manual. Is there any document including a higher detail level?
Thanks and best regards