This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Changing TBPRD value of slave EPWMs while sync enabled

Part Number: TMS320F28069M

EPWM1 is the master and EPWM2 is the slave in sync because I am doing phase shift between them.

EPWM1 is set at TBPRD=4500(10Khz) so if I change the EPWM2 TBPRD value =9000(5Khz).The action qualifier does not output anything. They work only when they are the same value or PHSEN is disabled(which I don't want).

My objective is:


1) Interrupt with EPWM1 at 10Khz (for calculations),SYNC disabled and (EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO ;)

2) EPWM2 AQ for switching at 5Khz but I want to change the phase to whatever I want with respect to EPWM1.

  • Hi Syed,

    EPWM1 is set at TBPRD=4500(10Khz) so if I change the EPWM2 TBPRD value =9000(5Khz).The action qualifier does not output anything. They work only when they are the same value or PHSEN is disabled(which I don't want).

    Can you please provide your initialization code for EPWM1 and EPWM2 so I can check what count mode you are using and what your action qualifier settings are? When you say "the action qualifier does not output anything", you mean you see EPWM2 at a constant low state?

    Best Regards,

    Marlyn

  • void
    InitEPwm1Example()
    {
    //
    // Setup TBCLK
    //
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO ; //
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;
    EPwm1Regs.TBPHS.half.TBPHS = 0;

    EPwm1Regs.TBPRD = 4500; //9000 // Set timer period 801 TBCLKs
    // EPwm1Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
    EPwm1Regs.TBCTR = 0x0000; // Clear counter

    //
    // Set Compare values
    //
    EPwm1Regs.CMPA.half.CMPA = 0; // Set compare A value
    EPwm1Regs.CMPB = 0; // Set Compare B value

    //
    // Setup counter mode
    //
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up

    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    //
    // Setup shadowing
    //
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
    EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Set actions
    //
    EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM1A on event A, up count
    EPwm1Regs.AQCTLA.bit.CAD = AQ_SET; // Clear PWM1A on event A, down count

    EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count
    EPwm1Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count

    //
    // Interrupt where we will change the Compare Values
    //
    EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_PRDZERO; // Select INT on Zero event
    EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT
    EPwm1Regs.ETPS.bit.INTPRD = 1; // Generate INT on 5th event

    //
    epwm1_info.EPwmRegHandle = &EPwm1Regs;

    }


    void
    InitEPwm2Example()
    {
    //
    // Setup TBCLK
    //
    EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // Pass through
    EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
    EPwm2Regs.TBPHS.half.TBPHS = 0;


    EPwm2Regs.TBPRD = 9000; //4500 // Set timer period 801 TBCLKs
    EPwm2Regs.TBCTR = 0x0000; // Clear counter

    //
    // Set Compare values
    //
    EPwm2Regs.CMPA.half.CMPA = 2000; // Set compare A value
    EPwm2Regs.CMPB = 0; // Set Compare B value

    //
    // Setup counter mode
    //
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up

    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    //
    // Setup shadowing
    //
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
    EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Set actions
    //
    EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM1A on event A, up count
    EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Clear PWM1A on event A, down count

    EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count
    EPwm2Regs.AQCTLB.bit.CBD = AQ_SET; // Clear PWM1B on event B, down count

    epwm2_info.EPwmRegHandle = &EPwm2Regs;

    }

    EPWM2 is constantly low when TBPRDs are different.
    as soon as I change them to the same value it starts working or if I disable sync it again starts to work.

  • Hi Syed,

    Please refer to this thread: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/801113/ccs-tms320f28379d-cannot-synchronize-different-epwm-frequencies 

    Essentially, you should switch the frequencies for EPWM1 and EPWM2 for proper synchronization.

    Best Regards,

    Marlyn