Part Number: TMS320F280039C
Other Parts Discussed in Thread: CONTROLSUITE
Hi Luo,
This is the continuation for the below thread
Hi thanks for the reply,
1. We followed the above document, and we successfully ported the code to 49c, and we spin the motor by using FAST and with Encoder (FYI: we spin the Estun_EMJ_04APB22_A motor with HV-kit).
2. As you already known that in HV-Kit there is only provision to connect Encoder A, B, R ( to Eqep).
And we observed that in the universal lab code rotor angle is calculated based on the pulse count (EQEP count).
3.We need to calculate the rotor position based on the encoder analog signals (C, D)(sine and cos signals).
4. Is there any example code to calculate the rotor position from encoder analog signals ?