Part Number: LAUNCHXL-F28027
Due to this error we are not able to flash the code to mcu with MATLAB. Can you please give some solution for flashing the code with MATLAB so that we can able to debug this by MATLAB obnly.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-F28027
Due to this error we are not able to flash the code to mcu with MATLAB. Can you please give some solution for flashing the code with MATLAB so that we can able to debug this by MATLAB obnly.
Currently, I am working using the launch pad F28027 (C2000 Piccolo) kit. I am working with MATLAB for the firmware development , i am able to generate the code from the MATLAB but when i am trying to flash the code into the microcontroller i am getting the below error.
Debug Server Scripting (DSS) error: SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder"
I tried to resolve this error but could not do so. please help with this error , i think this related to CCS.
However, I have installed all the required coding packages (MATLAB, Simulink and Embedded Coder) which are required to run. I think it is an error that due to the CCS software.
Vikas,
You have another thread on the same topic and I provided you the link. Did you follow through the link.
I will close this thread and let's debug further on that thread.
Thanks & Regards,
Santosh