This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: flash memory (SST39VF800A) access problem via XINTF

Part Number: TMS320F28335


Hi,

We have already using DUALPORT RAM and SARAM in our boards. They are working fine via XINTF. 

Now we want to use Microchip Brand Flash Ram which is SST39VF800A. All three memory must work on the board. You can see the timing configuration for all memories. I also configured the GPIOs as shown below. 

However when I looked the flash memory location from Memory Browser, I see all the values of flash memory is equal to 1. I can't change the flash memory values to 0. They always stay at 1. I tried to change the values via memory browser on debug mode. Where could i be doing wrong?

void ConfigXintf(void)
{
EALLOW;
// XINTF configuration
XintfRegs.XINTCNF2.bit.XTIMCLK = 0; // XTIMCLK = SYSCLKOUT = 150MHz
XintfRegs.XINTCNF2.bit.CLKMODE = 0; // XCLKOUT = XTIMCLK = 150 MHz
XintfRegs.XINTCNF2.bit.CLKOFF = 0; // Enable XCLKOUT
XintfRegs.XINTCNF2.bit.WRBUFF = 0; // No write buffering
XintfRegs.XINTCNF2.bit.HOLD = 1; // Does not grant a request to an external device
// ZONE 0 - Timing for 4k x16 Dualport SRAM Access
XintfRegs.XTIMING0.bit.XWRLEAD = 1; // zone write timing
XintfRegs.XTIMING0.bit.XWRACTIVE = 1;
XintfRegs.XTIMING0.bit.XWRTRAIL = 0;
XintfRegs.XTIMING0.bit.XRDLEAD = 1; // zone read timing
XintfRegs.XTIMING0.bit.XRDACTIVE = 2;
XintfRegs.XTIMING0.bit.XRDTRAIL = 0;
XintfRegs.XTIMING0.bit.X2TIMING = 0; // don't double all zone read/write lead/active/trail timing
XintfRegs.XTIMING0.bit.USEREADY = 0; // does not sample XREADY signal
XintfRegs.XTIMING0.bit.READYMODE = 0; // sample asynchronous
XintfRegs.XTIMING0.bit.XSIZE = 3; // configured for 16-bit mode
// ZONE 6 - Timing for 512k x16 Flash Access
XintfRegs.XTIMING6.bit.XWRLEAD = 3; // zone write timing
XintfRegs.XTIMING6.bit.XWRACTIVE = 7;
XintfRegs.XTIMING6.bit.XWRTRAIL = 3;
XintfRegs.XTIMING6.bit.XRDLEAD = 3; // zone read timing
XintfRegs.XTIMING6.bit.XRDACTIVE = 7;
XintfRegs.XTIMING6.bit.XRDTRAIL = 3;
XintfRegs.XTIMING6.bit.X2TIMING = 1; // double all zone read/write lead/active/trail timing
XintfRegs.XTIMING6.bit.USEREADY = 0; // does not sample XREADY signal
XintfRegs.XTIMING6.bit.READYMODE = 0; // sample asynchronous
XintfRegs.XTIMING6.bit.XSIZE = 3; // configured for 16-bit mode
// ZONE 7 - Timing for 512k x16 SRAM Access
XintfRegs.XTIMING7.bit.XWRLEAD = 1; // zone write timing
XintfRegs.XTIMING7.bit.XWRACTIVE = 0;
XintfRegs.XTIMING7.bit.XWRTRAIL = 0;
XintfRegs.XTIMING7.bit.XRDLEAD = 1; // zone read timing
XintfRegs.XTIMING7.bit.XRDACTIVE = 1;
XintfRegs.XTIMING7.bit.XRDTRAIL = 0;
XintfRegs.XTIMING7.bit.X2TIMING = 0; // don't double all zone read/write lead/active/trail timing
XintfRegs.XTIMING7.bit.USEREADY = 0; // does not sample XREADY signal
XintfRegs.XTIMING7.bit.READYMODE = 0; // sample asynchronous
XintfRegs.XTIMING7.bit.XSIZE = 3; // configured for 16-bit mode
// Bank switching
// Zone 6 is slow, so add additional BCYC cycles
// when ever switching from Zone 6 to another Zone.
// This will help avoid bus contention.
XintfRegs.XBANK.bit.BANK = 6;
XintfRegs.XBANK.bit.BCYC = 7;
EDIS;
//Force a pipeline flush to ensure that the write to
//the last register configured occurs before returning.
asm(" RPT #7 || NOP");
}

void InitDSPXintf16Gpio()
{
   EALLOW;

/* Configure XINTF pins using GPIO regs*/
   GpioCtrlRegs.GPCMUX1.bit.GPIO64 = 3;  	// XD15
   GpioCtrlRegs.GPCMUX1.bit.GPIO65 = 3;  	// XD14
   GpioCtrlRegs.GPCMUX1.bit.GPIO66 = 3;  	// XD13
   GpioCtrlRegs.GPCMUX1.bit.GPIO67 = 3;  	// XD12
   GpioCtrlRegs.GPCMUX1.bit.GPIO68 = 3;  	// XD11
   GpioCtrlRegs.GPCMUX1.bit.GPIO69 = 3;  	// XD10
   GpioCtrlRegs.GPCMUX1.bit.GPIO70 = 3;  	// XD19
   GpioCtrlRegs.GPCMUX1.bit.GPIO71 = 3;  	// XD8
   GpioCtrlRegs.GPCMUX1.bit.GPIO72 = 3;  	// XD7
   GpioCtrlRegs.GPCMUX1.bit.GPIO73 = 3;  	// XD6
   GpioCtrlRegs.GPCMUX1.bit.GPIO74 = 3;  	// XD5
   GpioCtrlRegs.GPCMUX1.bit.GPIO75 = 3;  	// XD4
   GpioCtrlRegs.GPCMUX1.bit.GPIO76 = 3;  	// XD3
   GpioCtrlRegs.GPCMUX1.bit.GPIO77 = 3;  	// XD2
   GpioCtrlRegs.GPCMUX1.bit.GPIO78 = 3;  	// XD1
   GpioCtrlRegs.GPCMUX1.bit.GPIO79 = 3;  	// XD0

   GpioCtrlRegs.GPBMUX1.bit.GPIO40 = 3;  	// XA0
   GpioCtrlRegs.GPBMUX1.bit.GPIO41 = 3;  	// XA1
   GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 3;  	// XA2
   GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 3;  	// XA3
   GpioCtrlRegs.GPBMUX1.bit.GPIO44 = 3;  	// XA4
   GpioCtrlRegs.GPBMUX1.bit.GPIO45 = 3;  	// XA5
   GpioCtrlRegs.GPBMUX1.bit.GPIO46 = 3;  	// XA6
   GpioCtrlRegs.GPBMUX1.bit.GPIO47 = 3;  	// XA7
   GpioCtrlRegs.GPCMUX2.bit.GPIO80 = 3;  	// XA8
   GpioCtrlRegs.GPCMUX2.bit.GPIO81 = 3;  	// XA9
   GpioCtrlRegs.GPCMUX2.bit.GPIO82 = 3;  	// XA10
   GpioCtrlRegs.GPCMUX2.bit.GPIO83 = 3;  	// XA11
   GpioCtrlRegs.GPCMUX2.bit.GPIO84 = 3;  	// XA12
   GpioCtrlRegs.GPCMUX2.bit.GPIO85 = 3;  	// XA13
   GpioCtrlRegs.GPCMUX2.bit.GPIO86 = 3;  	// XA14
   GpioCtrlRegs.GPCMUX2.bit.GPIO87 = 3;  	// XA15
   GpioCtrlRegs.GPBMUX1.bit.GPIO39 = 3;  	// XA16
   GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 3;  	// XA17
   GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 3;  	// XA18
   GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 3;  	// XA19

   GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 3;  	// XREADY
   GpioCtrlRegs.GPBMUX1.bit.GPIO35 = 3;  	// XRNW
   GpioCtrlRegs.GPBMUX1.bit.GPIO38 = 3;  	// XWE0
   GpioCtrlRegs.GPBMUX1.bit.GPIO36 = 3;  	// XZCS0
   GpioCtrlRegs.GPBMUX1.bit.GPIO37 = 3;  	// XZCS7
   GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 3;  	// XZCS6

   GpioCtrlRegs.GPBMUX2.bit.GPIO63 = 0; 	// Configure GPIO63 as GPIO63 (nSEMR for dualport memory)
   GpioCtrlRegs.GPBPUD.bit.GPIO63 = 0; 		// Enable pull-up on GPIO63 (nSEMR)
   GpioCtrlRegs.GPBDIR.bit.GPIO63 = 1;		// Configure GPIO63 as Output
   GpioDataRegs.GPBDAT.bit.GPIO63 = 1;		// Set nSEMR

   GpioCtrlRegs.GPBMUX2.bit.GPIO62 = 0; 	// Configure GPIO62 as GPIO62 (INTR for dualport memory)
   GpioCtrlRegs.GPBPUD.bit.GPIO62 = 0; 		// Enable pull-up on GPIO62 (INTR)
   GpioCtrlRegs.GPBDIR.bit.GPIO62 = 0;		// Configure GPIO62 as Input
   GpioDataRegs.GPBDAT.bit.GPIO62 = 1;		// Set INTR


   EDIS;
}

  • Ahmet,

                    Flash works very differently compared to RAM. While you can change any bit in RAM any way you want anytime you wish, it is not so simple with Flash. Flash memory uses a very different technology compared to RAM, which is what gives us the benefit of non-volatility. In the erased state, all bits in Flash are 1. Programming operation is where chosen bits are flipped to 0. Depending on the technology used to manufacture the Flash chip, a very specific sequence needs to be followed to program the flash (this is described in page 7 of the SST39VF200 datasheet). While we use the word "write" for RAM, we generally use the word "program" for flash. You can change the value of a bit from 1 to 0 but not the other way around. Also, you need to erase the flash before you can program it. Generally, you cannot erase a single byte/word; you need to erase an entire sector. Please go through the flash chip's datasheet very carefully. 

    I see all the values of flash memory is equal to 1.

    That is very likely because the flash chip is in an erased state.

    I can't change the flash memory values to 0. They always stay at 1

    You need to follow the specific sequence to erase/program the device.

    I tried to change the values via memory browser on debug mode.

    That will not work, for the reasons I already explained.